Hello everyone,
I have been working on a project to develop a simple power meter. I have mainly been working a simple DC circuit and a photo resister to measure the change in voltage of the simple circuit when covering up the resistor. It cause the resistance to fluctuate so I can measure a voltage of 0 to .3 volts. Now that I have that part working I'm trying to figure out how to go about attaching a split core current sensor . It produces a voltage up to .333 vols AC. My initial thought is to wire the black lead to ground and white lead to the pin that I'm sampling but then I realized that is what I would do for DC. Second thought was to wire each lead to different pins and alternate sampling between the two. I am now to the point where I honestly don't know what I'm doing and the rest of the team I am currently on doesn't have the vaguest idea of how to approach it either.
Thanks =)