Part Number: MSP-GANG
Other Parts Discussed in Thread: MSP430G2402, MSP430G2232
During this seemingly unending semiconductor shortage, I needed to change the microcontroller on an existing PCBA to one that was actually available to purchase. Ended up replacing an MSP430G2402 with an MSP430G2232. Our CM failed to notify me when the change occured in our scheduled deliveries of boards, and the received PCBA's weren't marked with the new revision, so our manufacturing line unknowingly used revised boards. We use an MSP-GANG programmer to program eight identical boards at once. The programmer successfully programmed the boards built with the MSP430G2232 even though the image was built for an MSP430G2402. I thought that the MSP-GANG would ID the microcontroller first and if there was a mismatch between the image and the one detected, that it would signal an error -- IT DIDN'T. Is this normal operation for the programmer?