Part Number: MSP430G2102
Hi,
Its to inform you that I have used MSP430G2102 microcontroller for the firmware development where i have used PORT1, PORT2, Timer, I2C examples code routine with the interrupt.
I have select the whole program optimization with speed 5.
While build the project, flash memory overflow shown of 250 bytes more. As total flash size is of 1 kb and during compilation flash memory overflow shown is of 1250 bytes.
But the same firmware build successfully using open source msp430-gcc. Here the flash used 988 bytes out of total flash size 1 KB.
So can u please give me the solution for the below 2 query:
1) Project Configuration settings of CCS helpful to build the firmware which is not able to build till now.
2) Why the firmware which is build successfully with open source msp430-gcc, failed to build with CCS?
Looking forward to hear from you as soon as possible.
Regards,
RRJ