This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430 Compiler error: Failed to get device

I'm using IAR Workbench for MSP430 7.21 compiler. When I was debugging, it gave me errors "Failed to get device"

How can I solve this problem?

Tue Jan 25, 2022 14:55:33: IAR
Embedded Workbench 7.21.1 (C:\
Program Files (x86)\IAR Systems\
Embedded Workbench 8.5\430\bin\
430proc.dll)
Tue Jan 25, 2022 14:55:33: Using
license: Network license:

Tue Jan 25, 2022 14:55:33: Firmware
version 3.4.1.0
Tue Jan 25, 2022 14:55:33: Interface dll
version 0.0.0.884
Tue Jan 25, 2022 14:55:33: Failed to
RegisterMessageCallback
Tue Jan 25, 2022 14:55:34: Device :
M703
Tue Jan 25, 2022 14:55:34: External
voltage : 3.3 V
Tue Jan 25, 2022 14:55:34: VCC voltage
: 3.3 V
Tue Jan 25, 2022 14:55:35: Failed to get
device
Tue Jan 25, 2022 14:55:35: Download
complete.
Tue Jan 25, 2022 14:55:35: Loaded
debugee:
Tue Jan 25, 2022 14:55:35: Failed to get
device
Tue Jan 25, 2022 14:55:35: Target reset
Tue Jan 25, 2022 14:55:35: Failed to get
device
Tue Jan 25, 2022 14:55:35: Failed to get
device
Tue Jan 25, 2022 14:55:35: Failed to get
device
Tue Jan 25, 2022 14:55:35: Failed to get
device

**Attention** This is a public forum