Hi,
I have a question from my customer.
Suppose ACLK source is XT1 LF (the default condition) and WDT-A is sourced from ACLK.
At device power-up, XT1 LF is not stabilized, so ACLK is automatically switched to REFOCLK, according to user's manual section 5.2.12 "UCS Module Fail-Safe Operation".
On the other hand, section 16.2.5 Clock Fail-Safe Feature in WDT-A says:
As ACLK is maintained thanks to the UCS fail-safe, I guess the fail-safe feature in WDT-A is not triggered at power-up.
So WDT-A is sourced from ACLK (REFOCLK) not VLOCLK.
Correct?
Thanks and regards,
Koichiro Tashiro