Part Number: MSP430FR2476
Other Parts Discussed in Thread: MSP430FR2355
Hello everyone,
I am trying to implement MSPBoot code for MSP430FR2476. I am using MSP430FRBoot document and MSP430FRBoot 1_03_00_00 examples. I have a few questions:
1- I am using Code Composer Studio. As i can see from "MSPBoot_FR2433_UART", there are custom target configurations(Example : BSLBased_16bit_UART). These configurations seem to be created automatically for the given device. How can I generate the configuration for the different device (MSP430FR2476)? What is the proper way?
2- There is a linkergen util that creates a linker file for the given device. But it seems like memory mappings are created according to the flash series. If I understand right, there are some wrong areas (like FLASH), and there are some missed areas (JTAGSIGNATURE, FRAM, etc.). Should users create linker files manually for FRAM devices? Is it okay to use linker files that are generated by linkergen? If yes why it is okay to use a flash-based linker and is it the proper way to use it?
Best Regards,
Ege