This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5529: Array issue

Part Number: MSP430F5529

Hi team,

Here's an issue from the customer may need your help:

Consumer intend to convert the data in 430 from 10 to binary and put it into an array. The following functions are available in the c-language editor, but the parameter is viewed in ccs and the array is 0 anyway. The customer also defines an additional equation: E=n+i; the result is also 0.

In following program, the seu [i] array is assigned and can be found in expression, but the j variable is still 0. The customer would like to know why is that.

Could you help check this case? Thanks.

Best Regards,

Cherry

**Attention** This is a public forum