This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2433: Firmware upgrade issue

Part Number: MSP430FR2433


Hi team,

Here's an issue may need your help:

The motor head has a bluetooth chip inside the tube which is the msp430 master motor, connected in serial to implement bluetooth control of the motor. Now we would like to do a wireless upgrade and to do a program upgrade to the msp430FR2433 over the serial port by taking advantage of the wireless upgrade feature of Bluetooth, the Bluetooth chip reads the upgrade package for the msp430.

Issues:

1)  implementation of the msp430FR2433 serial upgrade function, is there a DEMO program for serial upgrade?

2) serial port upgrade program space requirements for msp430 chip, currently used is msp430fr2433, total 15 k, motor control program already uses 10K.

Could you help check this case? Thanks.

Best Regards,

Cherry

**Attention** This is a public forum