Hi team,
Here's an issue from the customer may need your help:
As per the datasheet, the BSL must operate below the main frequency of 8 MHz. But the customer's debug results on the board are as follows:
If the chip is always running within 8 MHz, including 8 MHz, then the BSL is no problem. However, if the chip operates at 16 MHz first and then drops below 8 MHz before the BSL, the BSL will fail.
When sending default password, the following error will be reported:
[ACK_ERROR_MESSAGE]Unknown ACK value!
The customer would like to know how to resolve this issue. Could you help check this case? Thanks.
Best Regards,
Cherry