This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F6726: RTC function during low power mode

Part Number: MSP430F6726

Hi team

Our customer is developing their system with MSP430F6726, they are verifying RTC function with low power mode function. customer would like to change the operation mode to LPM3.5 in order to operate RTC, however, customer is not sure the difference between LPM3.5 configuration and LPM4.5 configuration, exactly. It seems customer is referring to the UserGuide " Table 1-2. Operation Modes ". Can I have your Expert's advice/comments on this inquiry, please?

And then, customer Is asking if OSCOFF in LPM3.5 mode is not "1" but "0".

It will be appreciated if you will share expert's comments.

Best regards,

Miyazaki

**Attention** This is a public forum