This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2355: eCOMP temp behavior and leakage current

Part Number: MSP430FR2355

Team,

A customer of mine would like to get more information about temperature dependency of the internal comparator. The datasheet only specifies a min/max value.

  • How stable is the offset with temperature?
  • What is the worst case input leakage to a comparator pin across the full temperature range? We need to use quite high impedance of around 100K hence we need to know the effect this will have to the errors as the offset is high at 30mV.

 

Thanks,
  Robert

**Attention** This is a public forum