This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
We recently have some FRAM data lost problems with our products using MSP430FR5994IZVWR.
The MCU was functioning properly at the beginning, while after running couple days(without reboot/reset), some of the MCU had the FRAM memory lost issues.
The memory allocation and partition is as shown below:
0x4000 ——0x17FFF:CODE1 (80KB)
0x18000——0x2BFFF:CODE2 (80KB)
0x2C000——0x437FF:DATA (94KB)
0x43800——0x43FFF:CODE3 (2KB)
The WPROT in the FRCTL0 register is set to be 0.
We used UniFlash to debug the FRAM issues and found that part of the data in CODE1 and all of the data in CODE2 were set to be 0xFF unexpected, and the data in DATA and CODE3 were still correct.
Once we reprogram the MCU, it works properly but the same problem happens accidentally.
We look forward to your reply and thank you for your time in advanced.
Thanks,
Chen
Hi Jian,
Have you enable the MPU module?
We recommend enable MPU to protect your code:
You can refer this example: https://dev.ti.com/tirex/explore/node?node=AP7nrlhk5xV4B0INSnZ6Iw__IOGqZri__LATEST
Thanks!
Best Regards
Johnson
Hi Jian,
I fthe MCU run whti over spec will cause some issue.
Like over voltage, voltage current, etc..
Thanks!
Best Regards
Johnson
The MPU can prevent a rogue pointer from trashing your code but it just masks the real problem. The most likely cause is a loop that doesn't terminate when it should which allows it to write over your code.
Using the MPU in a debug environment so you can examine the program state after it detects an attempt to write over your code would help you locate the problem. Or just a careful look at your code and loop termination criteria.
**Attention** This is a public forum