Part Number: MSP430FR2632
Hi,
I need to write a routine, in order to check each individual pin of my MSP.
To check the GPIO pins, it's relatively easy, I configure it as an input, the neighbours are configured as high level output, and I check if I get a high input, which means I have a soldering short between some pins.
anyway, this is not the problem.
Now, I want to check the captivate pins, in order to now if they are cut somewhere on the PCB.
How can I get a value from those pins (sometime purely captivate pins, sometime alternate function can be GPIO) ?
(I have 6 pins to check, it is a 3x3 track pad)
Thanks for you help.