This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2544: Production burn failed

Part Number: MSP430G2544

Hi team,

Here's an issue may need your help:

1) The following is a platform built during the burn process using the programr MSP430 GANG PROGRAMMER, Auto 2.7V Dongle, which is a board-level burn and the burning fixture.

2) Burning S/W, Sermac is developed by the customer.

3) Target supply voltage 2.7 V during the burn process, supplied by the programmer, and the burning fixture's power is off.

Testing: after a non-burn issue, try to power the board from an external source. But still cannot be burned.

Could you help check this case? Thanks.

Best Regards,

Cherry

**Attention** This is a public forum