Part Number: MSP430F5436A
Hello,
We use MSP430F5436A and LF crystal CM7V-T1A-12.5pF for the 32.768kHz..
With some boards and sometimes we face stalled LF crystal at power up. A reset or a power down then up does not change anything. The same board can start correctly a few hours after then stay stalled the day after...
Reading the document slaa322d.pdf, at chapter 2.1 I can see: "Hence, if using two equal capacitors, the values of these capacitors must be twice the required load capacitance."
So with XCAP configured at 12pF inside the MSP430F5436A, can I consider that the CM7V-T1A-12.5pF is the correct choice or must I use CM7V-T1A-7.0pF ?
Best regards and many thanks for any suggestions
Mich