Im working on a project on my msp430g2452 device and I am using P1.0, 1.3, 1.4, 1.5, 1.6, and 1.7 for adc10. I have all the ports configured fine but P1.7 is stuck at 3.4V and P1.5, 1.4, and 1.3 are all around 2V. All the other pins i want to use for adc10 are fine. I have even tried a new very basic project to turn the ports on and off and they are still stuck. Is something wrong with my device?