This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-GANG: Error 63: Target not open

Part Number: MSP-GANG

Hello,

we use the MSP-GANG.dll  in our application.

Our flashing strategy based on mode "From Image File".  (.mspgangimage)

string imageFilePath = /.../.../imageName.mspgangimage

MSPGANG.SetConfig(ConfigIndexes.CFG_PROJECT_SOURCE, ConfigIndexes.FROM_IMAGE_FILE_MODE);

MSPGANG.SetConfig(ConfigIndex.FROMIMAGE_BIT, 0x1000);

MSPGANG.ImageFileLoad(imageFilePath, null, 0);

MSPGANG.InteractiveProcess(1000);

MSPGANG.GetProgressStatus(pnt);

Now and again we observe during the flashing action an interruption the flashing action with error message:

     Error 63:  Target not open

Erase, Blank check, Write : are ok

Verify : not ok 

Beginning of verify operation cause the upper error message.

What could be the cause of the error message?

Regards,

Paul

**Attention** This is a public forum