This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5994: Error connecting to the target

Part Number: MSP430FR5994
Other Parts Discussed in Thread: MSP-FET

Hi Experts,

A customer Is receiving the error MSP430: Error connecting to the target: Unknown device when trying to upload a code to their custom board using the MSP-FET emulator this via CCS.

Can you help check if the schematic is correct or if there are any errors?

Please find the attached schematic file for your reference.

CMS_X011_Sch (2).pdf

Thank you.

Regards,

Marvin

  • Hi Marvin,

    The schematic looks fine.

    Ask the customer how long are the programming signal paths from the MSPFET to the target MSP (this includes length of wires + traces on PCB)?  If > 20cm have them try shortening the wires.

    Is the target MSP powered from the MSPFET or separate power source during programming?

  • Hi Marvin,

    It's been a while since we have heard from you, so I'm going to assume you were able to move forward with your project.
    I will mark this posting as RESOLVED, but if this isn’t the case, please click the "This did NOT resolve my issue" button and reply to this thread with more information.
    If this thread is locked, please click the "Ask a related question" button, and in the new thread describe the current status of your issue and any additional details you may have to assist us in helping to solve your issues.

**Attention** This is a public forum