Part Number: MSP430FR5962
Hi experts,
Q1:Is there any errata information on standard functions that are not specifically mentioned in the TI compiler user's manual?
Standard functions are functions that are only described as "supported," such as C99. We need information on potential bugs that are not listed in the above documents.
Q2:When implementing software (when using libraries including standard functions), what method should be used to determine if the function or library to be implemented can be used?
I understand that I need to check at least the following documents:
Device user's guide, datasheets, and errata. Compiler and assembly language user's guides
We also need information on the above to eliminate potential bugs, etc. by not using functions that cannot be used (or are not supported) in the first place.
Please point out if my explanation is insufficient.
Best regards,
O.H