Part Number: LDCTOUCHCOMCOILEVM
Hi Team,
We are integrating touch controller GT928 with imx8mm in Android 11 code base.
We need confirmation on following two points:
1. Can you provide I2C Register address for gt928.
2. Apart from DTSI changes, what are the changes required to configure I2C slave address?
As per data sheet GT928 supports two I2C slave addresses: 0xBA/0xBB and 0x28/0x29. The host can select the address by changing the status of Reset and INT pins during the power-on initialization phase".
For power-on initialization phase, Do we need to make any changes in driver or DTSI changes would be enough ?
Thnaks
Divyesh