This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2355: Where is the order of module function defined?

Part Number: MSP430FR2355


On page 335 in the MSP430 Family User Guide (SLAU445I), the order for the function selection register PxSEL1 is give as

  • (00=0) GPIO
  • (01=1) Primary
  • (10=2) Secondary
  • (11=3) Tertiary  

If I look at the pin diagram and its description for P4.3 given in MSP430FR235x Datasheet (SLASEC4D), I would assume the order of pin functions are arranged accordingly:

  • (00=0) GPIO = P4.3 I/O
  • (01=1) Primary = UCA1TXD
  • (10=2) Secondary = UCA1SIMO
  • (11=3) Tertiary = ~UCA1TXD


If I configure that P4.3 pin as my UART's Tx, I would of naturally thought that I should set my selector to be 01b or 11b if my logic is inverted.  But then I came across page 17 on the datasheet, the PSEL is actually 01b or 10b instead.   So the function selection order does not correspond to the order in the pin diagram, and instead we have this order

  • (00=0) GPIO = P4.3 I/O
  • (01=1) Primary = UCA1TXD
  • (10=2) Secondary = ~UCA1TXD
  • (11=3) Tertiary = UCA1SIMO

Where and in which documentation can I find the order of functions for a pin? 

**Attention** This is a public forum