This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5969-SP: working with ADC128S102WGMPR

Part Number: MSP430FR5969-SP

Hi Team,

The customer is building a system to be launched to the aerospace and would want to use ADC128S102WGMPR with MSP430FR5969-SP to sample 4 ADC channels with 250kHz. 

It looks like the ADC can do 1MHz, so it is possible to have 1M/4 = 250kHz. But the customer is worried about the MSP430 being not fast enough to produce the SPI 16M clock, as well as 16 bits data shift.

Can you confirm whether these two chips can work together or if not, can you suggest some other radiation-hardened microcontrollers can do this work?

Thanks!

Regards,

Marvin

**Attention** This is a public forum