Part Number: MSP430FR5994
Other Parts Discussed in Thread: MSP-EXP430FR5994
I am writing some code for the MSP430FR5994 (specifically the MSP-EXP430FR5994), and I am following the sample code for sending a PC signal and back. In order to use the USB port on the EXP board, I need to change the UART pins from P6.0 and 6.1 to P2.0 and P2.1. The following is the code that I have changed to achieve this.
#include <msp430.h>
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop Watchdog
// Configure GPIO
P2SEL0 &= ~(BIT0 | BIT1);
P2SEL1 |= (BIT0 | BIT1); // USCI_A0 UART operation (p93_s)
P6SEL1 &= ~(BIT0 | BIT1);
P6SEL0 |= (BIT0 | BIT1); // USCI_A3 UART operation (p109_s)
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
// Startup clock system with max DCO setting ~8MHz
CSCTL0_H = CSKEY_H; // Unlock CS registers
CSCTL1 = DCOFSEL_3 | DCORSEL; // Set DCO to 8MHz
CSCTL2 = SELA__VLOCLK | SELS__DCOCLK | SELM__DCOCLK;
CSCTL3 = DIVA__1 | DIVS__1 | DIVM__1; // Set all dividers
CSCTL0_H = 0; // Lock CS registers
// Configure USCI_A3 for UART mode
//UCA3CTLW0 = UCSWRST; // Put eUSCI in reset (p788)
//UCA3CTLW0 |= UCSSEL__SMCLK; // CLK = SMCLK
// Baud Rate calculation
// 8000000/(16*9600) = 52.083
// Fractional portion = 0.083
// User's Guide Table 21-4: UCBRSx = 0x04
// UCBRFx = int ( (52.083-52)*16) = 1
//UCA3BRW = 52; // 8000000/16/9600, BRW = Baud Rate Ctrl Word Register, p789
//UCA3MCTLW |= UCOS16 | UCBRF_1 | 0x4900; // UCOS16 = Oversampling enable, used when high frequency clk is used, probably divides everything by 16, UCBRF = fine turner when UCOS16 is active
// 0x4900 is for first 8 bits,
//UCA3CTLW0 &= ~UCSWRST; // Initialize eUSCI
//UCA3IE |= UCRXIE; // Enable USCI_A3 RX interrupt
// Configure USCI_A0 for UART mode
UCA0CTLW0 = UCSWRST; // Put eUSCI in reset (p788)
UCA0CTLW0 |= UCSSEL__SMCLK; // CLK = SMCLK
// Baud Rate calculation for 19200
// 8000000/(16*19200) = 26.042
// Fractional portion = 0.042
// User's Guide Table 21-4: UCBRSx = 0x04
// UCBRFx = int ( (52.083-52)*16) = 1
UCA0BRW = 52; // 8000000/16/9600, BRW = Baud Rate Ctrl Word Register, p789
UCA0MCTLW |= UCOS16 | UCBRF_1 | 0x4900; // UCOS16 = Oversampling enable, used when high frequency clk is used, probably divides everything by 16, UCBRF = fine turner when UCOS16 is active
// 0x4900 is for first 8 bits,
UCA0CTLW0 &= ~UCSWRST; // Initialize eUSCI
UCA0IE |= UCRXIE; // Enable USCI_A0 RX interrupt
__bis_SR_register(LPM3_bits | GIE); // Enter LPM3, interrupts enabled
__no_operation(); // For debugger
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=EUSCI_A0_VECTOR
__interrupt void USCI_A0_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(EUSCI_A0_VECTOR))) USCI_A0_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(UCA0IV, USCI_UART_UCTXCPTIFG))
{
case USCI_NONE: break;
case USCI_UART_UCRXIFG:
while(!(UCA0IFG&UCTXIFG)); //While the A0 flag and TX flag are not both active
UCA0TXBUF = UCA0RXBUF;
__no_operation();
break;
case USCI_UART_UCTXIFG: break;
case USCI_UART_UCSTTIFG: break;
case USCI_UART_UCTXCPTIFG: break;
default: break;
}
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=EUSCI_A3_VECTOR
__interrupt void USCI_A3_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(EUSCI_A3_VECTOR))) USCI_A3_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(UCA3IV, USCI_UART_UCTXCPTIFG))
{
case USCI_NONE: break;
case USCI_UART_UCRXIFG:
while(!(UCA3IFG&UCTXIFG)); //While the A3 flag and TX flag are not both active
UCA3TXBUF = UCA3RXBUF;
__no_operation();
break;
case USCI_UART_UCTXIFG: break;
case USCI_UART_UCSTTIFG: break;
case USCI_UART_UCTXCPTIFG: break;
default: break;
}
}
However, I am unable to transmit a character from my PC to the board using Termite. Testing the system with pins 6.0 and 6.1, with the GPIO pins connected to the J101 pins are effective in changing it.