This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F4784: Program running only in debug

Part Number: MSP430F4784

Hi,

Currently I'm using MSP430F4784. To test the controller is working I simply programmed LED blink.

When ran this program in debug mode it worked fine. However, when the debugger is stopped and I reset the controller the LED is not blinking and also there is no voltage in output.

To confirm I cross checked in various pins but the results are same.

What would be the issue?

Is there any change I need to do in properties? 

**Attention** This is a public forum