Part Number: MSP430FR5994
I have these two h-files:
- MSP430F5XX_F6XXGENERIC.h
- MSP430FR5994.h
Some registers are properly named in one file and others in the other file. Specifically the adc12_b files seem to be correct in the device-specific h-file, while timer_a seems to be correct in the Generic h-file.
For example, in the library timer_a.c file, the register offset OFS_TAxCCR0 is used, which is defined in the Generic file. But the device-specific file defines OFS_TA0CCR0. Both have the same offset value (0x12).
If I include both files, I get warnings for duplicate definitions of other registers.
What is the correct way to manage these two files?
Thanks!
Dan