Part Number: MSP430FG6426
Dear Team,
I have MSP430FG6426 actuating around 80 inductive loads (each 25mA) activated through a comination of TI's 74HC595 shift register and ULN2803.
I get the debug session running very fine while activating the ULN channels in the manner i want.
But when i try to connect the load of the 80 inductive loads, the debug session gets messed up with an error "MSP430: Trouble Halting Target CPU", and this happens all the time when i try to switch ON more than 10 solenoids here. (if i keep it less than 10 then i have no issues)
Another point here is that, i dont see any issues with the controller and its able to run without any issues even if all 80 loads are activated. Its just the debugger that fails at this time.
I am using Code composer - 9.2.0
Debugger- MSPFET430UIF with SpyBiWire

Would be really helpful if i can get a clue here why the debugger misbehaves ?
Thanks
Surya