Part Number: MSP430F5131
Other Parts Discussed in Thread: MSP430F5132
Hi Experts!
I tried to build any ADC example code for the MSP430F5131. The code example I want to use is MSP430F51x2_ADC10_07.c
However, this is a problem with all ADC10 example codes. The issue is ADC10 registers are not defined in the #include <msp430> header.

After I add #include <msp430F5132.h> (which defines all the registers ADC10CTL0, ADC10SHT_2,...), I still get a similar but different error.
Now, ADC10CTLx registers are undefined.

(Side note: I did not #include F5131.h files because these files do not define registers ADC10CTL0, ADC10SHT_2,...)
Is there another header file I must include? Wanted to raise awareness of this issue that all MSP430F5131 ADC examples will not build out of box.