Other Parts Discussed in Thread: MSP430F5528, UNIFLASH
Hello,
I'm working on the "Optimized Ultrasonic Sensing Metrology Water Flow Measurement Reference Design" project on EVM430-FR6043. I built and ran the code on the board, but when I launch the Ultrasonic Sensing Design Center Interface and try to connect it, I get the error: "No connected HID devices".
In principal, I configured jumpers correctly for Design Center communication (J1: 1-2 ON, 3-4: ON, 5-6: ON, 7-8: OFF and 9-10: OFF). Also, I configured jumpers so the board is powered by USB. The rest of jumpers haven't been touched since I bought the kit.
Thanks in advance,
Alberto