Part Number: MSP430FR2433
Hi Ti!
I am designing a battery powered sensor with the MSP430FR2433IYQW.
I need to have an idea (during the sensor operation life) of the battery status.
1-) Is it a good idea to use the SVS to know the battery status ?
I ask because the MSP430FR2433IYYQW has no battery monitor, only SVS.
2-) Is it possible to generate 16MHz on the DCOCLK from XT1 (32,768KHz) ?
My intention is to have a stable frequency (16MHz) in DCOCLK to achieve UART without failures.
Thank you very much. Best regrads