Part Number: MSP430FR5043
Hi,
I am using the library (Lobe Wide and Hilbert Wide) provided by TI with the following settings.
・ PATTERN_SEQ_MULTI_TONE (multitone: 2 frequencies)
・ USS_ALG_ABS_TOF_COMPUTATION_MODE_HILBERT_WIDE (HilbWide algorithm)
・ USS_ALG_FILT_IS_FILTER_ENABLED (BP-Filter enabled)
As a result of changing to the Hilbert Wide library by referring to the following document to reduce the memory, it was confirmed that the memory is reduced.
However, all the measurement results will be "0".
Even if I change to another library (Hilbert, Lobe, LobeWide), the measurement result is "0", and currently only Lobe Wide and Hilbert Wide can operate normally.
Is there any change required to use the Hilbert Wide version, such as changing the Config parameter specified in the USS library?
Thanks,
Astro