This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5244: 'ERROR 58: Verification Error' occurs when download program by using MSP-GANG

Part Number: MSP430F5244
Other Parts Discussed in Thread: MSP430F5418A,

Hi team,

Here's an issue from the customer may need your help:

programmer : MSP-GANG

mode : BSL

The 9 of 200pcs boards download failed, and the program is empty when using MSP-GANG to read it from chip at this time.

These boards are mounted in the same batch of SMT. These MCUs are the same batch as well.

The specific error reported by the MSP-GANG programmer is as follows:


Executing Main Process...
.............
  2 : Get Password
  3 : Get Password
  4 : init target
  5 : Loading FBSL
  6 : Starting FBSL
  7 : erasing-Info
  8 : erasing-Info
  9 : erasing-Info
 10 : erasing-Main
 11 : erasing-Main
 12 : erasing-Main
 13 : erasing-Main
 14 : erasing-Main
 15 : Blank-1800
 16 : Blank-1880
 17 : Blank-1900
 18 : Blank-4400
 19 : Blank-8000
 20 : Blank-10000
 21 : Blank-18000
 22 : Blank-20000
 23 : Write-4400
 24 : Write-8000
 25 : Write-FFDC
 26 : Write-FFE2
 27 : Write-FFEA
 28 : Write-FFF0
 29 : Write-FFFE
 30 : 
ERROR 58: Verification Error
Failed
ERROR 58: Verification Error


Thanks.

Best Regards,

Yale Li

**Attention** This is a public forum