Part Number: MSP430G2553
Hi, I use msp430g2553 for my project that implement on CCS, but I have some problems. I use the i2c protocol to communicate between MSP and vl53l5cx (ToF sensor of ST) - my i2c doesn't have interrupt. 2 timer interval are used WDT timer, TIMER0_A0 and 1 interrupt timer PORT2 with P2.0 pin.
After a several time, it stuck on <while( (!(IFG2 & UCB0TXIFG))/> so I use time_out counter to continue, but it's still stuck, I think my code for init timer and interrupt is not good. Can you check for me?
/* I2C */
I2C_Mode I2C_Master_ReadReg(uint8_t dev_addr, uint16_t reg_addr, uint8_t *rxBuff, uint32_t count)
{
/* Initialize state machine */
i2cMasterMode = I2C_TX_REG_ADDRESS_MODE;
i2cReceiveBuffer = rxBuff;
isTransmitRegAddr = true;
i2cTransmitRegAddr = reg_addr;
i2cRXByteCtr = count;
i2cTXByteCtr = 0;
i2cReceiveIndex = 0;
i2cTransmitIndex = 0;
bool waitRx = true;
uint8_t rx_val = 0;
uint16_t i_timeout = 0; //minhnvk
/* Initialize slave address and interrupts */
UCB0I2CSA = dev_addr;
IFG2 &= ~(UCB0TXIFG + UCB0RXIFG); // Clear any pending interrupts
UCB0CTL1 |= UCTR + UCTXSTT; // I2C TX, start condition
i_timeout = 0;
while( (!(IFG2 & UCB0TXIFG)) && i_timeout <=65000) //minhnvk
{
i_timeout ++;
if(i_timeout == 65000)
return 99;
}
UCB0TXBUF = (i2cTransmitRegAddr & 0xFF00) >> 8;
i_timeout = 0;
while( (!(IFG2 & UCB0TXIFG)) && i_timeout <=65000) //minhnvk
{
i_timeout ++;
if(i_timeout == 65000)
return 99;
}
UCB0TXBUF = (i2cTransmitRegAddr & 0xFF);
i_timeout = 0;
while( (!(IFG2 & UCB0TXIFG)) && i_timeout <=65000) //minhnvk
{
i_timeout ++;
if(i_timeout == 65000)
return 99;
}
// IE2 &= ~UCB0TXIE; // Disable TX interrupt //minhnvk cmt 7-4
UCB0CTL1 &= ~UCTR; // Switch to receiver
UCB0CTL1 |= UCTXSTT; // Send repeated start
if (i2cRXByteCtr == 1)
{
//Must send stop since this is the N-1 byte
i_timeout = 0;
while((UCB0CTL1 & UCTXSTT) && i_timeout <= 65000)
{
i_timeout ++;
if(i_timeout == 65000)
return 99;
}
UCB0CTL1 |= UCTXSTP; // Send stop condition
}
while(waitRx)
{
i_timeout = 0;
while( (!(IFG2 & UCB0RXIFG)) && i_timeout <=65000)
{
i_timeout++;
if(i_timeout == 65000)
return 99;
}
{
rx_val = UCB0RXBUF;
if (i2cRXByteCtr)
{
i2cReceiveBuffer[i2cReceiveIndex++] = rx_val;
i2cRXByteCtr--;
}
if (i2cRXByteCtr == 1)
{
UCB0CTL1 |= UCTXSTP;
}
else if (i2cRXByteCtr == 0)
{
IE2 &= ~UCB0RXIE; //minhnvk cmt 7-4
i2cMasterMode = I2C_IDLE_MODE;
waitRx = false;
}
}
}
return i2cMasterMode;
}
I2C_Mode I2C_Master_WriteReg(uint8_t dev_addr, uint16_t reg_addr, uint8_t *reg_data, uint32_t count)
{
/* Initialize state machine */
i2cMasterMode = I2C_TX_REG_ADDRESS_MODE;
isTransmitRegAddr = true;
i2cTransmitRegAddr = reg_addr;
//Copy register data to TransmitBuffer
i2cTransmitBuffer = reg_data;
i2cTXByteCtr = count;
i2cRXByteCtr = 0;
i2cReceiveIndex = 0;
i2cTransmitIndex = 0;
bool waitTx = true;
uint16_t i_timeout = 0; //minhnvk
/* Initialize slave address and interrupts */
UCB0I2CSA = dev_addr;
IFG2 &= ~(UCB0TXIFG + UCB0RXIFG); // Clear any pending interrupts
UCB0CTL1 |= UCTR + UCTXSTT; // I2C TX, start condition
i_timeout = 0;
while( (!(IFG2 & UCB0TXIFG)) && i_timeout <=65000) //minhnvk
{
i_timeout ++;
if(i_timeout == 65000)
return 99;
}
UCB0TXBUF = (i2cTransmitRegAddr & 0xFF00) >> 8;
i_timeout = 0;
while( (!(IFG2 & UCB0TXIFG)) && i_timeout <=65000) //minhnvk
{
i_timeout ++;
if(i_timeout == 65000)
return 99;
}
UCB0TXBUF = (i2cTransmitRegAddr & 0xFF);
while(waitTx)
{
i_timeout = 0;
while( (!(IFG2 & UCB0TXIFG)) && i_timeout <=65000) //minhnvk
{
i_timeout ++;
if(i_timeout == 65000)
return 99;
}
if (i2cTXByteCtr)
{
UCB0TXBUF = i2cTransmitBuffer[i2cTransmitIndex++];
i2cTXByteCtr--;
}
else
{
//Done with transmission
UCB0CTL1 |= UCTXSTP; // Send stop condition
i2cMasterMode = I2C_IDLE_MODE;
// IE2 &= ~UCB0TXIE; // disable TX interrupt
waitTx = false;
}
}
return i2cMasterMode;
}
void initGPIOI2C()
{
// P1DIR |= BIT0 + BIT1 + BIT2 + BIT3 + BIT4;
// P1OUT &= ~(BIT0 + BIT1 + BIT2 + BIT3 + BIT4);
// P2OUT &= ~BIT5;
// P2OUT &= ~BIT2;
// P2DIR |= BIT5 + BIT2;
// P2OUT |= BIT5;
// P2OUT &= ~BIT2;
// __delay_cycles(1600000);
// P2OUT &= ~BIT5;
// P2OUT |= BIT2;//reset sensor slave
P1OUT &= ~BIT0;
P2OUT &= ~BIT2;
P2DIR |= BIT2;
P1DIR |= BIT0;
P1OUT |= BIT0;
P2OUT &= ~BIT2;
// __delay_cycles(1600000);
P1OUT &= ~BIT0;
P2OUT |= BIT2;//reset sensor master
P1SEL |= BIT6 + BIT7; // Assign I2C pins to USCI_B0
P1SEL2|= BIT6 + BIT7; // Assign I2C pins to USCI_B0
}
void initI2C()
{
UCB0CTL1 |= UCSWRST; // Enable SW reset
UCB0CTL0 = UCMST + UCMODE_3 + UCSYNC; // I2C Master, synchronous mode
UCB0CTL1 = UCSSEL_2 + UCSWRST; // Use SMCLK, keep SW reset
UCB0BR0 = 40; // fSCL = SMCLK/160 = ~400kHz
UCB0BR1 = 0;
UCB0I2CSA = SLAVE_ADDR; // Slave Address
// UCB0CTL1 &= ~UCSWRST; // Clear SW reset, resume operation
// UCB0I2CIE |= UCNACKIE;
}
void I2Cinit(){
initI2C();
initGPIOI2C();
UCB0CTL1 &= ~UCSWRST;
}
/* WDT timer and Timer0_A0 */
void setup_TimerA0(){
BCSCTL1 = CALBC1_16MHZ; // Set DCO to 1MHz
DCOCTL = CALDCO_16MHZ;
WDTCTL = WDT_MDLY_8; // Set Watchdog Timer interval to ~8ms
// IE1 |= WDTIE; // Enable WDT interrupt
TA0CTL |= TASSEL_3 + MC_1; //Interved TACLK, Continuous MODE
TA0CCR0 = 10000;
TA0CCTL0 = CCIE;
}
#pragma vector = TIMER0_A0_VECTOR
__interrupt void TimerInterruptCCR0(void){
__disable_interrupt();
count++;
// processTimerEvent();
if(StatusLed == FUZZY_LED)
{
counter++;
if(counter == 5)
{
P2OUT &= ~BIT3;
counter = 0;
}
else
P2OUT |= BIT3;
}
__enable_interrupt();
}
/* Watchdog Timer interrupt service routine*/
#pragma vector=WDT_VECTOR
__interrupt void watchdog_timer(void)
{
__disable_interrupt();
if(TA0R < last_tc)
{
TempCnt = 0;
}
else
{
TempCnt = TA0R - last_tc;
}
if((GetMeasureTouch_delta() > Threshold))
dem++;
else
dem = 0;
if(dem > 5)
buttonPress = true;
else
buttonPress = false;
last_tc = TA0R;
__enable_interrupt();
// TA0CTL |= TACLR; //Clear Timer_A TAR
}
/* PORT2 interrupt */
void initInterrupt(void)
{
//slave to initiate transfer -
P2DIR &= ~BIT0; // Set P2.0 to inpput direction
P2REN |= BIT0; // Enable P2.0 internal resistance
P2OUT |= BIT0; // Set P2.0 as pull-Up resistance
P2IES |= BIT0; // P2.0 Hi/Lo edge
P2IFG &= ~BIT0; // P2.0 IFG cleared
P2IE |= BIT0; // P2.0 interrupt enabled
InteruptState = FallingEdge;
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=PORT2_VECTOR
__interrupt void Port_2(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(PORT2_VECTOR))) Port_2 (void)
#else
#error Compiler not supported!
#endif
{
__disable_interrupt();
if(InteruptState == FallingEdge)
{
TimeInterupt = getTickCount();
InteruptState = RisingEdge;
P2IES &= ~BIT0; // P2.0 Hi/Lo edge
// P2IE |= BIT0; // P2.0 interrupt enabled
i =99;
}
else if (InteruptState == RisingEdge)
{
i = getTickCount() - TimeInterupt;
P2IES |= BIT0; // P2.0 Hi/Lo edge
InteruptState = FallingEdge;
}
switch(i)
{
case 1: case 2:
StatusSlave = NONE_DETECT_SLAVE;
break;
case 3: case 4:
StatusSlave = DETECT_SLAVE;
break;
case 5: case 6:
slave_bright_level = slave_bright_high;
break;
case 7: case 8:
StatusSlave = BTN_SLAVE;
break;
case 9: case 10:
slave_bright_level = slave_bright_low;
break;
default:
break;
}
P2IFG &= ~BIT0; // P2.0 IFG cleared
P2IE |= BIT0; // P2.0 interrupt enabled
__enable_interrupt();
}