Other Parts Discussed in Thread: MSP430FR6989, MSP-FET
I have used this Launchpad in past and worked well to flash a firmware on MsP430FR6989 microcontroller using CCS 8.3.1.
Now when I am repeating the same actions with the same Launchpad and microcontroller using CCS 8.3.1, it asks for firmware update of Launchpad.
Stating, ”Error initializing emulator: A firmware update is required for the MSP430 Debug Interface (MSP-FET430UIF / MSP-FET / eZ-FET).”
If I ignore the update, CCS responds “Error connecting to the target: Unknown device”.
If I update the firmware, CCS responds “Error connecting to the target: Internal Error”.
The simple example like blinkLED do not work on the board now! The device when connected with PC, lights up the green power LED.
I would like more information on how to use this Launchpad now.