Part Number: EVM430-FR6043
Dear TI,
Good morning!
Please help me to find out the solution of below problems.
1) "DToF -shift was greater than maximum sample shift"
This above error is displaying again and again. Please help me to overcome this issue.
Although, I have been tried to change the "USS_ALG_MAX_SAMPLE_SHIFT " value from 20 to 40 in source code header file " USS_userconfig.h " to escape this error.
2) My flow tube is L-shaped and have one reflective surface inside the tube. I have used Audiowell 200KHz ultrasonic transducers and propagation length between both the transducers is ~135mm.
Please help me to overcome the issue of instability of volume reading on EVM6043 and also the ADC value as shown below figures.