Part Number: MSP430F5529
Hi Champ,
I am asking for my customer. They are working on update process issue, and I get confused with their process.
The process is Switch to Flash BSL(0x1000) → Write RAM BSL to RAM(0x2500) → Switch to RAM BSL(0x2500) → Program App into Flash(0x4400) → Switch to App(0x4400).
Flash BSL:BSL_00.08.88.39.txt (Use MSP430Flasher.exe to read from the chip, and then compare)
RAM BSL:RAM_BSL_00.07.08.38.txt
The update process does not support the function of restoring the FW after the update process is powered off, and both the Flash BSL and the RAM BSL are official images.
In general, most of the customers implement the update process that the RAM BSL will be omitted, and the APP will be updated directly through the Flash BSL.
May I consult the purpose for doing the way like this which has any special consideration ? Or is it recommended from any our doc. ?
Thanks and regards.