This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2311: Problem of code conversion between 2 MSP430

Part Number: MSP430FR2311
Other Parts Discussed in Thread: MSP430FR2433

Hello, 

I am currently working on a system which can measure the variable frequency (100Hz - 2MHz) of a square signal. The MCU I use for my system is a MSP430FR2311.

I found on dev.ti.com (link below) a code which can measure the frequency of a signal. This application is done with a MSP430FR2433. In this application, you put a square signal of 5kHz at the input and you can get the frequency thanks to the code. 

Link of the application I found : Timer - Capture Mode


As I said, I am working with a MSP430FR2311. I checked the datasheets and modified the registers to make the code work (I didn't modify comments in my C file, so comments still talk about FR2433 device). Sadly, I can't find out why this doesn't work for me. I can build the project but nothing happens when I look at the different variables signalFreq and timerAcaptureValues (which is TimerB, I didn't modify the name of the expression), neither when I put a 5kHz signal at the input, nor when I try to use the first part of the code on the website, using the auxiliary clock as the input signal.
Can you help me figure out why my code doesn't work and help me to make it work ? You can find the C file attached.

/* --COPYRIGHT--,BSD_EX
 * Copyright (c) 2014, Texas Instruments Incorporated
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 *
 *******************************************************************************
 *
 *                       MSP430 CODE EXAMPLE DISCLAIMER
 *
 * MSP430 code examples are self-contained low-level programs that typically
 * demonstrate a single peripheral function or device feature in a highly
 * concise manner. For this the code may rely on the device's power-on default
 * register values and settings such as the clock configuration and care must
 * be taken when combining code from several examples to avoid potential side
 * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
 * for an API functional library-approach to peripheral configuration.
 *
 * --/COPYRIGHT--*/
//***************************************************************************************
//  MSP430FR24xx Demo - Timer0_A3 Capture of ACLK
//
//  Description: Capture a number of periods of the ACLK clock and store them in an array.
//  When the set number of periods is captured the program is trapped and the LED on
//  P1.0 is toggled. At this point halt the program execution read out the values using
//  the debugger.
//  ACLK = REFOCLK = 32kHz, MCLK = SMCLK = default DCODIV = 1MHz.
//
//                MSP430FR2433
//             -----------------
//         /|\|                 |
//          | |             P1.2|<-- TA0.CCI2A
//          --|RST              |  |
//            |             P2.2|--> ACLK
//            |                 |
//            |             P1.0|-->LED
//
//
//  Wei Zhao
//  Texas Instruments Inc.
//  Jan 2014
//  Built with IAR Embedded Workbench v6.20 & Code Composer Studio v6.0.1
//***************************************************************************************
#include <msp430.h>

#define NUMBER_TIMER_CAPTURES        20

volatile unsigned int timerAcaptureValues[NUMBER_TIMER_CAPTURES];
unsigned int timerAcapturePointer = 0;

int main(void)
{
    WDTCTL = WDTPW | WDTHOLD;                       // Stop watchdog timer

    // Configure GPIO
    P1DIR |= BIT0;                                  // Set P1.0 as output
    P1OUT |= BIT0;                                  // P1.0 high
    P1SEL1 |= BIT2;                                 // TA0.CCI2A input capture pin, second function
    P1REN |= BIT2;                                  // enable internal pull-down resistor
    P1OUT &= ~BIT2;

    P2SEL1 |= BIT2;                                 // Set as ACLK pin, second function
    P2DIR |= BIT2;

    // Disable the GPIO power-on default high-impedance mode to activate
    // previously configured port settings
    PM5CTL0 &= ~LOCKLPM5;

    // Configure clock
    __bis_SR_register(SCG0);                        // disable FLL
    CSCTL3 |= SELREF__REFOCLK;                      // Set REFO as FLL reference source
    CSCTL0 = 0;                                     // clear DCO and MOD registers
    CSCTL1 &= ~(DCORSEL_7);                         // Clear DCO frequency select bits first
    CSCTL1 |= DCORSEL_2;                            // Set DCO = 4MHz
    CSCTL2 = FLLD_1 + 60;                           // DCODIV = 2MHz
    __delay_cycles(3);
    __bic_SR_register(SCG0);                        // enable FLL
    while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1));      // Poll until FLL is locked

    CSCTL4 = SELMS__DCOCLKDIV | SELA__REFOCLK;      // set default REFO(~32768Hz) as ACLK source, ACLK = 32768Hz
                                                    // default DCODIV as MCLK and SMCLK source
    CSCTL5 |= DIVM__1 | DIVS__2;                    // SMCLK = 1MHz, MCLK = 2MHz

    // Timer0_A3 Setup
    TB0CCTL2 |= CM_1 | CCIS_0 | CCIE | CAP | SCS;
                                                    // Capture rising edge,
                                                    // Use CCI2A=ACLK,
                                                    // Synchronous capture,
                                                    // Enable capture mode,
                                                    // Enable capture interrupt

    TB0CTL |= TBSSEL_2 | MC_2 | TBCLR;              // Use SMCLK as clock source, clear TA0R
                                                    // Start timer in continuous mode

    __bis_SR_register(LPM0_bits | GIE);
    __no_operation();
}

// Timer0_A3 CC1-2, TA Interrupt Handler
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector = TIMER0_B1_VECTOR
__interrupt void TIMER0_B1_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(TIMER0_B1_VECTOR))) TIMER0_B1_ISR (void)
#else
#error Compiler not supported!
#endif
{
    switch(__even_in_range(TB0IV,TB0IV_TBIFG))
    {
        case TB0IV_NONE:
            break;                                  // No interrupt
        case TB0IV_TBCCR1:
            break;                                  // CCR1 not used
        case TB0IV_TBCCR2:
            timerAcaptureValues[timerAcapturePointer++] = TB0CCR2;
            if (timerAcapturePointer >= 20)
            {
                while (1)
                {
                    P1OUT ^= 0x01;                  // Toggle P1.0 (LED)
                    __delay_cycles(100000);
                }
            }
            break;                                  // CCR2 not used
        case TB0IV_TBIFG:
            break;                                  // overflow
        default:
            break;
    }
}


Thank you by advance, 

Best regards, 

Ghilain

**Attention** This is a public forum