Part Number: EVM430-FR6047
We are currently evaluating the correction using "VFR Flow+Temperarure".
I have a question about the temperature that is being estimated from absoluteTOF in it.
When we check the calculation results, we are able to measure the water temperature with an accuracy of ±0.5 to 1°C compared to the actual measured value at 10°C to 20°C. However, at 40°C to 50°C, the error is around -4°C.
Do you know the cause?
Also, please let us know if there are any countermeasures.
Also, if possible, I would like a reply by e-mail.
Best regards
Masaki Kubota