This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR4132: Cannot connect MSP-FET with CCS

Part Number: MSP430FR4132
Other Parts Discussed in Thread: MSP-FET,

Hello all, I'm trying to debug with MSP-FET.

When I start debugging with MSP-FET, I get an error message "Error connecting to the target: Unknown device".
What could be the cause of this?

The development environment is CCS version 10.4.0.00006.
The CPU is MSP430FR4132.

The following figure is an excerpt from the circuit diagram.

The 4-wire JTAG and RST,TEST are connected.

Properties are shown in the figure below.

TIMSP430USB1 is selected for connection..

The following figure is Target configs.

Thank you very much.
Suzuki

**Attention** This is a public forum