This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2744: Timer A3 Usage

Part Number: MSP430G2744

Hi Team,

My customer has a question regarding the use of timer A3. Is the below images correct for 1) starting the timer and 2) stopping the timer?

They want to use the timer in compare mode with the timer source being SMCLK = 1.15MHz using TACCTL2 and TACCR2 registers.

1) 

2) 

Also, in the start sequence, is there supposed to be a wait time or is it not necessary for the wait? If it is necessary, can you tell me how long?

Best regards,

Mari Tsunoda

  • For using the timer I would advise your customer to refer to this code example:

    /* --COPYRIGHT--,BSD_EX
     * Copyright (c) 2012, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *
     *******************************************************************************
     * 
     *                       MSP430 CODE EXAMPLE DISCLAIMER
     *
     * MSP430 code examples are self-contained low-level programs that typically
     * demonstrate a single peripheral function or device feature in a highly
     * concise manner. For this the code may rely on the device's power-on default
     * register values and settings such as the clock configuration and care must
     * be taken when combining code from several examples to avoid potential side
     * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
     * for an API functional library-approach to peripheral configuration.
     *
     * --/COPYRIGHT--*/
    //******************************************************************************
    //  MSP430G2x44 Demo - Timer_A, PWM TA1-2, Up Mode, DCO SMCLK
    //
    //  Description: This program generates two PWM outputs on P1.2,3 using
    //  Timer_A configured for up mode. The value in TACCR0, 512-1, defines the PWM
    //  period and the values in TACCR1 and TACCR2 the PWM duty cycles.
    //  Using ~1.2MHz SMCLK as TACLK, the timer period is ~425us with
    //  a 75% duty cycle on P1.2 and 25% on P1.3.
    //  ACLK = n/a, SMCLK = MCLK = TACLK = default DCO ~1.2MHz
    //
    //               MSP430G2x44
    //            -----------------
    //        /|\|              XIN|-
    //         | |                 |
    //         --|RST          XOUT|-
    //           |                 |
    //           |         P1.2/TA1|--> TACCR1 - 75% PWM
    //           |         P1.3/TA2|--> TACCR2 - 25% PWM
    //
    //  William Goh
    //  Texas Instruments Inc.
    //  March 2013
    //  Built with CCS Version: 5.3.0 and IAR Embedded Workbench Version: 5.51
    //******************************************************************************
    #include <msp430.h>
    
    int main(void)
    {
      WDTCTL = WDTPW + WDTHOLD;                 // Stop WDT
      P1DIR |= 0x0C;                            // P1.2 and P1.3 output
      P1SEL |= 0x0C;                            // P1.2 and P1.3 TA1/2 otions
      TACCR0 = 512 - 1;                         // PWM Period
      TACCTL1 = OUTMOD_7;                       // TACCR1 reset/set
      TACCR1 = 384;                             // TACCR1 PWM duty cycle
      TACCTL2 = OUTMOD_7;                       // TACCR2 reset/set
      TACCR2 = 128;                             // TACCR2 PWM duty cycle
      TACTL = TASSEL_2 + MC_1;                  // SMCLK, up mode
    
      __bis_SR_register(CPUOFF);                // Enter LPM0
    }
    
    

    For stop the timer, you can refer to this. I think customer's setting is right.

**Attention** This is a public forum