Other Parts Discussed in Thread: MSP-FET, , MSP-GANG
Dear sir/madam,
In our design we have used MSP430FR2355TRHAR MCU. We have below queries:
Query No. 01 ) For Analog input channel, MCU 12-bit analog to digital converter (ADC) is used. For ADC, internal 2.5V voltage reference is used.
In case of this internal 2.5V voltage reference used,
-- pin no. 02 (Veref+) and pin no. 40 (Veref-) should be left open as unused pin or should connect any circuit at these pins? If yes, which circuit use?
-- pin no. 25 (VREF+) should be left open as unused pin or should connect any circuit at this pin. If yes, which circuit use?
Query No.02) How should be simplified Block diagram / Architecture of MCU 12-bit analog to digital converter (ADC).Please share the same.
Query No.03) How should be simplified Block diagram / Architecture of MCU 12-bit digital to analog converter (DAC) mode. Please share the same.
Query No.04) Whether the RST from the debugger is a CMOS type or an open drain type? Please share the reference document which shows Debugger RST pin details.
Request, please share the reply/answers for above queries.
Thanks & Regards
Rohidas Sawant | MEI