Part Number: MSP430F67791A
We are using Ti controller series MSP430F67791A in our Protection relay device .I have already connected a crystal of 32.768kHz with Load Capacitance of 15pF and generated ADC interrupt of 1ms to collect ADC sample in every 1 ms. But due to accuracy concern we could not able to collect the each sample in 1 ms duration.
Some time it collect in 2ms , 1.3, 0.980 , 0.550 & 0.002. Which affect our measurement magnitude & relay operating time value. Hence forth we would like to use 8.00MHz crystal with same controller is it feasible to configure the clock initialization and ADC interrupt using 8.00MHz crystal.
If so, then what are the parameters alongwith parameter values that we need to be taken into consideration???
We are waiting for your quick response which will help us to move forward.
Thanks & Regards.
Kaustubh Gawli