Part Number: MSP430FR6989
Hello,
I am uisng a 16MHz clock. My question is that if I use the "__delay_cycles();" function, what is the higiest value that I can use in it? for example,
int i;
//Wait 5 seconds
for(i=0;i<5;i++)
{
__delay_cycles(16000000);
}
If I use this code, I'll get a 5 second delay as my clock frequency is 16MHz. What is the maximum value that I can put in the "__delay_cycles();" function without using the for loop and why?
Thank You.