This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2422: how to control MSP gang programmer from another microcontroller in a test jig.

Part Number: MSP430FR2422


how to control MSP gang programmer from another microcontroller in a test jig.

My requirement 

I have two firmware files one for testing and one actual firmware file, I am planning to do an automation process during production and testing of my circuit which consist MSP 430 controller, now I want a way to command the programmer to download specific firmware (either test firmware or actual code based on testing status), the test jig consist of an 8bit microcontroller which should be able to command and also check for program status.

**Attention** This is a public forum