Part Number: MSP430F5232
Hello everyone,
I´m working on the MSP430 doing basic stuff as sending and receiving UART, polling is working perfectly if i check in the while(1) but the interrupt is never triggered, i´ve tried both this example and the driverlib example with none firing the interrupt.
//******************************************************************************
// MSP430F524x Demo - USCI_A0, UART Echo received character
// (ACLK 9600/SMCLK 9600/SMCLK 115200)
//
// Description: The device will wait in LPM0/LPM3 (based on clock source)
// until a UART character is received.
// Then the device will echo the received character.
// The UART can operate using ACLK at 9600, SMCLK at 115200 or SMCLK at 9600.
// To configure the UART mode, change the following line:
//
// #define UART_MODE SMCLK_115200
// to any of:
// #define UART_MODE SMCLK_115200
// #define UART_MODE SMCLK_9600
// #define UART_MODE ACLK_9600
//
// UART RX ISR is used to handle communication.
// ACLK = 32.768kHz, MCLK = SMCLK = DCO 16MHz.
//
//
// MSP430F5249
// -----------------
// /|\ | P5.4|--- XIN
// | | | |
// ---|RST | 32kHz
// | | |
// | P5.5|--- XOUT
// | P3.4|<------- Receive Data (UCA0RXD)
// | P3.3|-------> Transmit Data (UCA0TXD)
// | |
// | |
//
// Nima Eskandari and Ryan Meredith
// Texas Instruments Inc.
// January 2018
// Built with CCS V7.3
//******************************************************************************
#include "msp430.h"
#include <stdbool.h>
#include <stdint.h>
//******************************************************************************
// UART Initialization *********************************************************
//******************************************************************************
#define SMCLK_115200 0
#define SMCLK_9600 1
#define ACLK_9600 2
#define UART_MODE SMCLK_115200//SMCLK_115200//
void initUART()
{
// Configure USCI_A0 for UART mode
UCA0CTLW0 = UCSWRST; // Put eUSCI in reset
#if UART_MODE == SMCLK_115200
UCA0CTLW0 |= UCSSEL__SMCLK; // CLK = SMCLK
// Baud Rate calculation
// 16000000/(16*115200) = 8.6805
// Fractional portion = 0.6805
// Use Table 24-5 in Family User Guide
UCA0BR0 = 8; // 16000000/16/9600
UCA0BR1 = 0x00;
UCA0MCTL |= UCOS16 | UCBRF_11 | UCBRS_0;
#elif UART_MODE == SMCLK_9600
UCA0CTLW0 |= UCSSEL__SMCLK; // CLK = SMCLK
// Baud Rate calculation
// 16000000/(16*9600) = 104.1667
// Fractional portion = 0.1667
// Use Table 24-5 in Family User Guide
UCA0BR0 = 104; // 16000000/16/9600
UCA0BR1 = 0x00;
UCA0MCTL |= UCOS16 | UCBRF_3 | UCBRS_0;
#elif UART_MODE == ACLK_9600
UCA0CTLW0 |= UCSSEL__ACLK; // CLK = ACLK
// Baud Rate calculation
// 32768/(9600) = 3.4133
// Fractional portion = 0.4133
// Use Table 24-5 in Family User Guide
UCA0BR0 = 3; // 32768/9600
UCA0BR1 = 0x00;
UCA0MCTL |= UCBRS_3; //0x0300 is UCBRSx = 0x03
#else
# error "Please specify baud rate to 115200 or 9600"
#endif
UCA0CTLW0 &= ~UCSWRST; // Initialize eUSCI
UCA0IE |= UCRXIE; // Enable USCI_A0 RX interrupt
}
//******************************************************************************
// Device Initialization *******************************************************
//******************************************************************************
void initGPIO()
{
P3SEL = BIT3 | BIT4; // P3.4,5 = USCI_A0 TXD/RXD
P5SEL |= BIT4 | BIT5; // Select XT1
}
void initClockTo16MHz()
{
UCSCTL3 |= SELREF_2; // Set DCO FLL reference = REFO
UCSCTL4 |= SELA_0; // Set ACLK = XT1CLK
__bis_SR_register(SCG0); // Disable the FLL control loop
UCSCTL0 = 0x0000; // Set lowest possible DCOx, MODx
UCSCTL1 = DCORSEL_5; // Select DCO range 16MHz operation
UCSCTL2 = FLLD_0 + 487; // Set DCO Multiplier for 16MHz
// (N + 1) * FLLRef = Fdco
// (487 + 1) * 32768 = 16MHz
// Set FLL Div = fDCOCLK
__bic_SR_register(SCG0); // Enable the FLL control loop
// Worst-case settling time for the DCO when the DCO range bits have been
// changed is n x 32 x 32 x f_MCLK / f_FLL_reference. See UCS chapter in 5xx
// UG for optimization.
// 32 x 32 x 16 MHz / 32,768 Hz = 500000 = MCLK cycles for DCO to settle
__delay_cycles(500000);//
// Loop until XT1,XT2 & DCO fault flag is cleared
do
{
UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG); // Clear XT2,XT1,DCO fault flags
SFRIFG1 &= ~OFIFG; // Clear fault flags
}while (SFRIFG1&OFIFG); // Test oscillator fault flag
}
uint16_t setVCoreUp(uint8_t level){
uint32_t PMMRIE_backup, SVSMHCTL_backup, SVSMLCTL_backup;
//The code flow for increasing the Vcore has been altered to work around
//the erratum FLASH37.
//Please refer to the Errata sheet to know if a specific device is affected
//DO NOT ALTER THIS FUNCTION
//Open PMM registers for write access
PMMCTL0_H = 0xA5;
//Disable dedicated Interrupts
//Backup all registers
PMMRIE_backup = PMMRIE;
PMMRIE &= ~(SVMHVLRPE | SVSHPE | SVMLVLRPE |
SVSLPE | SVMHVLRIE | SVMHIE |
SVSMHDLYIE | SVMLVLRIE | SVMLIE |
SVSMLDLYIE
);
SVSMHCTL_backup = SVSMHCTL;
SVSMLCTL_backup = SVSMLCTL;
//Clear flags
PMMIFG = 0;
//Set SVM highside to new level and check if a VCore increase is possible
SVSMHCTL = SVMHE | SVSHE | (SVSMHRRL0 * level);
//Wait until SVM highside is settled
while((PMMIFG & SVSMHDLYIFG) == 0)
{
;
}
//Clear flag
PMMIFG &= ~SVSMHDLYIFG;
//Check if a VCore increase is possible
if((PMMIFG & SVMHIFG) == SVMHIFG)
{
//-> Vcc is too low for a Vcore increase
//recover the previous settings
PMMIFG &= ~SVSMHDLYIFG;
SVSMHCTL = SVSMHCTL_backup;
//Wait until SVM highside is settled
while((PMMIFG & SVSMHDLYIFG) == 0)
{
;
}
//Clear all Flags
PMMIFG &= ~(SVMHVLRIFG | SVMHIFG | SVSMHDLYIFG |
SVMLVLRIFG | SVMLIFG |
SVSMLDLYIFG
);
//Restore PMM interrupt enable register
PMMRIE = PMMRIE_backup;
//Lock PMM registers for write access
PMMCTL0_H = 0x00;
//return: voltage not set
return false;
}
//Set also SVS highside to new level
//Vcc is high enough for a Vcore increase
SVSMHCTL |= (SVSHRVL0 * level);
//Wait until SVM highside is settled
while((PMMIFG & SVSMHDLYIFG) == 0)
{
;
}
//Clear flag
PMMIFG &= ~SVSMHDLYIFG;
//Set VCore to new level
PMMCTL0_L = PMMCOREV0 * level;
//Set SVM, SVS low side to new level
SVSMLCTL = SVMLE | (SVSMLRRL0 * level) |
SVSLE | (SVSLRVL0 * level);
//Wait until SVM, SVS low side is settled
while((PMMIFG & SVSMLDLYIFG) == 0)
{
;
}
//Clear flag
PMMIFG &= ~SVSMLDLYIFG;
//SVS, SVM core and high side are now set to protect for the new core level
//Restore Low side settings
//Clear all other bits _except_ level settings
SVSMLCTL &= (SVSLRVL0 + SVSLRVL1 + SVSMLRRL0 +
SVSMLRRL1 + SVSMLRRL2
);
//Clear level settings in the backup register,keep all other bits
SVSMLCTL_backup &=
~(SVSLRVL0 + SVSLRVL1 + SVSMLRRL0 + SVSMLRRL1 + SVSMLRRL2);
//Restore low-side SVS monitor settings
SVSMLCTL |= SVSMLCTL_backup;
//Restore High side settings
//Clear all other bits except level settings
SVSMHCTL &= (SVSHRVL0 + SVSHRVL1 +
SVSMHRRL0 + SVSMHRRL1 +
SVSMHRRL2
);
//Clear level settings in the backup register,keep all other bits
SVSMHCTL_backup &=
~(SVSHRVL0 + SVSHRVL1 + SVSMHRRL0 + SVSMHRRL1 + SVSMHRRL2);
//Restore backup
SVSMHCTL |= SVSMHCTL_backup;
//Wait until high side, low side settled
while(((PMMIFG & SVSMLDLYIFG) == 0) &&
((PMMIFG & SVSMHDLYIFG) == 0))
{
;
}
//Clear all Flags
PMMIFG &= ~(SVMHVLRIFG | SVMHIFG | SVSMHDLYIFG |
SVMLVLRIFG | SVMLIFG | SVSMLDLYIFG
);
//Restore PMM interrupt enable register
PMMRIE = PMMRIE_backup;
//Lock PMM registers for write access
PMMCTL0_H = 0x00;
return true;
}
bool increaseVCoreToLevel2()
{
uint8_t level = 2;
uint8_t actlevel;
bool status = true;
//Set Mask for Max. level
level &= PMMCOREV_3;
//Get actual VCore
actlevel = PMMCTL0 & PMMCOREV_3;
//step by step increase or decrease
while((level != actlevel) && (status == true))
{
if(level > actlevel)
{
status = setVCoreUp(++actlevel);
}
}
return (status);
}
//******************************************************************************
// Main ************************************************************************
// Enters LPM0 if SMCLK is used and waits for UART interrupts. If ACLK is used *
// then the device will enter LPM3 mode instead. The UART RX interrupt handles *
// the received character and echoes it. *
//******************************************************************************
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop Watchdog
initGPIO();
increaseVCoreToLevel2();
initClockTo16MHz();
initUART();
P1DIR &= ~0x06; //pines del puerto de programación BSL: configurados como entradas.
P6DIR |= 0x08u; // configure P1.0 as output
P6OUT |= 0x08u; // toggle P1.0
long i=0;
while(1)
{
P6OUT ^= 0x08u; // toggle P1.0
switch(__even_in_range(UCA0IV,4))
{
case 0:break; // Vector 0 - no interrupt
case 2: // Vector 2 - RXIFG
while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready?
//UCA0TXBUF = UCA0RXBUF; // TX -> RXed character commented to use interrupt.
break;
case 4:break; // Vector 4 - TXIFG
default: break;
}
}
}
//******************************************************************************
// UART RX Interrupt ***********************************************************
//******************************************************************************
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_A0_VECTOR
__interrupt void USCI_A0_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_A0_VECTOR))) USCI_A0_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(UCA0IV,4))
{
case 0:break; // Vector 0 - no interrupt
case 2: // Vector 2 - RXIFG
while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready?
UCA0TXBUF = UCA0RXBUF; // TX -> RXed character
break;
case 4:break; // Vector 4 - TXIFG
default: break;
}
}
This code works perfectly fine at 115200 baud polling in the main but the interrupt is never triggered and Im out of ideas.