Other Parts Discussed in Thread: ADS1232REF, ADS1232, TL431
Hello,
I currently designinig a MSP430 based weigh scale and, I read the application note provided by Texas, but in this part I can't understand these mathematics used by the autor,
he says: For a 2mv/V weigh scale powered by a 3V battery we have a full - scale of : 3V * 2mV/V = 6mV for 10Kg, well, the he says:
Our weigh will have 10000 counts.
Well then I thinked, If we have 10000 counts, and the full load is 10kg, and the resolution is 1g, the voltage for 1g is : 6mV / 10000 * 1 = 0,6uV, well great, this is the same logic what I thinked.
But followingf he says: In order to resolve 1g the LSB voltage should be four times small than 0,6uV, then 0,15uV...
If for 1g is equal to 0,6uV and my A/D can measure this voltage for 1 count, why the autor divided it by 4?
this is link for application note, the page is 2.
http://focus.ti.com/lit/an/slaa220/slaa220.pdf
Thanks for any help.
Felipe