Part Number: MSP430F4784
Hi,
I'm currently using MSP430F4784.
Here I'm using DCO clock, which is 8MHz.
I want to increase the clock 12 - 16MHz.
what are the possible ways to get the desired clock in MSP430F4784.
Below given is clock initialization.
/** clock config **/
SCFQCTL |= SCFQ_4M;
SCFI0 |= FN_2;
FLL_CTL0 |= DCOPLUS;
/** for MCLK **/
FLL_CTL1 &= ~XT2OFF;
do
{
IFG1 &= ~OFIFG;
__delay_cycles(1000);
}while(IFG1 & OFIFG);
FLL_CTL1 &= ~SELS; // DCO for SMCLK
FLL_CTL1 |= SELM1; // XT2 for MCLK
FLL_CTL2 |= XT2S_2;