Part Number: MSP430FR6989
Other Parts Discussed in Thread: MSP-FET
Hi,
I'm currently using MSP430FR6989.
CCS 6.2.0 and #build 6.2.0.00050.
programmer - MSP-FET.
connected the JTAG as per the datasheet information.
Able to detect the MSP430FR6989.
But while loading hex I'm getting the below error only.
MSP430: File Loader: Verification failed: Values at address 0x04400 do not match Please verify target memory and memory map.
MSP430: GEL: File: C:\Users\Administrator\workspace_v6_2\eiu_tesst\Debug\eiu_tesst.out: a data verification error occurred, file load failed.
checked power 3.3V only also RST is pulled up.
what is the possible way to get out from this issue.
Thanks in advance.