Part Number: MSP430I2040
Other Parts Discussed in Thread: MSP430I2041
I generate default code from EnergyMeasurementDesignCenter tools with chip select MSP430I2041. After generated code compile with CCS and change target chip to MSP430I2040. Load code to EVM controller.
As per calibration documentation provided by
I download and install
open calibration-config.xml and change com port.

I don't understand the com port setting. line no 266 com port is set as per our console shown in PC device manager. Other two comport in line no 269 and 275 one for reference meter and one for generator need to change or not. Also this meter type id need to change?
After that I open application "calibrator-20121120.exe"

Calibration not successful between EVM and PC. I send log also
Starting
0: Meter thread started - com17 at 9600 baud
0: Serial open com17
Generator thread
Generator thread A - 8
Generator thread pts3_3c
0: Serial opened com17
0: Set tracing 0
Opening generator port cnca1
Cannot open generator serial port 'cnca1'
0: No valid response from UUT
0: No valid response from UUT
0: No valid response from UUT
How to resolved this problem and start calibration.