This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F22x4 - ADC10 Sample Example doubt

In the following sample code given by TI:

//******************************************************************************
//  MSP430F22x4 Demo - ADC10, Sample A11, Lo_Batt, Set P1.0 if AVcc < 2.3V
//
//  Description: A single sample is made on A11 (AVcc/2) with reference to
//  internal 1.5V Vref. Software sets ADC10SC to start sample and conversion
//  - ADC10SC automatically cleared at EOC. ADC10 internal oscillator times
//  sample (16x) and conversion. ADC10BUSY flag is polled for EOC. If A11
//  (AVcc/2) < 0311h (1.15V) indicating AVcc is less 2.3V, P1.0 set indicating
//  a lo_Batt condition, else reset.
//
//                MSP430F22x4
//             -----------------
//         /|\|              XIN|-
//          | |                 |
//          --|RST          XOUT|-
//            |                 |
//            |A11 (AVcc/2) P1.0|-->LED
//
//  A. Dannenberg
//  Texas Instruments Inc.
//  April 2006
//  Built with CCE Version: 3.2.0 and IAR Embedded Workbench Version: 3.41A
//******************************************************************************
#include "msp430x22x4.h"
 
void main(void)
{
  WDTCTL = WDTPW + WDTHOLD;                 // Stop WDT
  ADC10CTL1 = INCH_11;                      // AVcc/2
  ADC10CTL0 = SREF_1 + ADC10SHT_2 + REFON + ADC10ON;
  TACCR0 = 30;                              // Delay to allow Ref to settle
  TACCTL0 |= CCIE;                          // Compare-mode interrupt
  TACTL = TASSEL_2 + MC_1;                  // TACLK = SMCLK, Up mode
  __bis_SR_register(CPUOFF + GIE);          // LPM0, TA0_ISR will force exit
  TACCTL0 &= ~CCIE;                         // Disable timer Interrupt
  P1DIR |= 0x01;                            // Set P1.0 to output direction
 
  for (;;)
  {
    ADC10CTL0 |= ENC + ADC10SC;             // Sampling and conversion start
    while (ADC10CTL1 & ADC10BUSY);          // ADC10BUSY?
    if (ADC10MEM < 0x311)                   // ADC10MEM = A11 > 1.15V?
      P1OUT |= 0x01;                        // Set P1.0 LED on
    else
      P1OUT &= ~0x01;                       // Clear P1.0 LED off
  }
}
 
#pragma vector=TIMERA0_VECTOR
__interrupt void TA0_ISR(void)
{
  TACTL = 0;                                // Clear Timer_A control registers
  LPM0_EXIT;                                // Exit LPM0 on return
}

 

 

How is 0311hexadecimal equivalent to 1.15 V ?

 

 

  • The project uses 1.5V internal reference source.

    You see the description of the sample code like below. 

    //  Description: A single sample is made on A11 (AVcc/2) with reference to 
    //  internal 1.5V Vref. Software sets ADC10SC to start sample and conversion  

    That is why, 0x311 / 0x400 * 1.5 V = 1.1499 V. 

    This works well. 

  • Kusanagi is right about the mathematical part (well, not exaclty, as the resolution it VREF/0x3FF, not 0x400, since 0x3FF equals the reference, so the trigger point is 1.151V, but that's minor).

    However, the comment is misleading. The expression in the IF statement is trie, if the voltage is <1.151V, not >1.15V. So if that was what was confusing you, you're right, it IS wrong. And misleading, if you don't know better how the ADC works.

**Attention** This is a public forum