Hello,
I am wondering if the symbol/footprint issue from this post:
was resolved. The current Altium symbol script, when ran as of 7/25/22, does not match datasheet.
-Andrew
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am wondering if the symbol/footprint issue from this post:
was resolved. The current Altium symbol script, when ran as of 7/25/22, does not match datasheet.
-Andrew
Hi Andrew, I checked on the status and apparently it has not been completed. I contacted the responsible person and will let you know when the corrected symbol has been updated and available for download.
Thank you Dennis. You can confirm that the symbol from TI is incorrect, yeah? That the datasheet is correct and the auto-generated symbol from TI for Altium is incorrect? That's our main holdup right now, if the datasheet is wrong or the symbol is wrong. For example, in the ZVW BGA package, B11 is AVCC1 (per datasheet) and not P2.0_TB0.6_UCA0TXD... (per TI symbol).
Hi Andrew,
I have just reached out to the responsible engineer with your questions.
Andrew,
Confirmed datasheet is correct, symbol is wrong.
I'll let you know when update to symbol is available, although it sounds like you are moving forward without it.
**Attention** This is a public forum